HAT 28
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
- products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol .
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:Read the operating instructions before use. |
|
Instructions for use and other useful information |
|
Dealing with recyclable materials |
|
Do not dispose of electric equipment and batteries as household waste |
Symbols in the illustrations
The following symbols are used in illustrations:These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
|
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
|
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
|
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:Wear a hard hat |
|
Wear eye protection |
|
Wear protective gloves |
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationPull-out tester HAT 28 Generation 01 Serial no.
Safety
Safety instructions
Basic information concerning safety WARNING! Read all safety precautions and other instructions. Failure to observe the safety instructions and other instructions can result in damage to the tool and/or serious injury.Keep all safety precautions and instructions for future reference.
Proper preparation of the working area
- Keep your workplace clean and well lit. Cluttered or poorly lit workplaces invite accidents.
- Wear personal protective equipment and always wear protective goggles.
- It is recommended that rubber gloves and non-skid shoes are worn when working outdoors.
- Keep children clear. Keep everyone clear of your work zone.
- When working on walls or ceilings, make sure that the surrounding work area is secured. Falling objects or tools could cause serious injury.
- Avoid unusual body positions. Maintain firm footing and balance at all times. This will give you better control of the product in unexpected situations.
- Use product, accessories, insert tools, etc. in accordance with these instructions. Take the working conditions and the work to be performed into account. Use of equipment for applications other than those intended can result in hazardous situations.
- To reduce the risk of injury, use only genuine Hilti tools and accessories.
- Follow the instructions concerning care and maintenance.
- Never tamper with or modify the power tool in any way.
- The tool is intended for professional use. The tool may be operated, serviced and repaired only by authorized, trained personnel. This personnel must be specially informed of any possible hazards.
- Do not operate the machine if your full attention is not on the job.
Description
Product overview
- Grip
- Crank
- Coupling
- Pressure gauge
- Tester housing
- Load distribution bridge
- Swiveling feet
- Adapter X-IE
- Slotted button adapter
- Threaded button adapter
- Scaffold ringbolt adapter
- Button adapter
- Threaded-rod adapter
- Threaded-rod legs
- Loading claw foot
- Spacer, small
- Spacer, large
Intended use
The product described is an application-specific system for testing fasteners. It consists of a mechanical screw jack passing through a hydraulic load cell which directly measures the load applied to the fastener and shows this read-out on the pressure gage.
There is a range of HAT 28 kits. These kits have been specially assembled for testing most small and medium-size fasteners.Items supplied
Pull-out tester, operating instructionsOther system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Overview of spacers for the stud welding application
Stud length (effective thread length) |
Spacer used |
---|---|
≤ 25 mm |
No spacer needed. |
≤ 38 mm |
Use small spacer. |
≤ 50 mm |
Use large spacer. |
≤ 100 mm |
Use large spacer and small spacer together. |
Technical data
HAT 28 DX |
HAT 28 M |
HAT 28 S/SR |
||
---|---|---|---|---|
Maximum displacement |
50 mm |
50 mm |
50 mm |
|
Displacement indicator scale |
mm |
mm |
mm |
|
Housing |
Aluminum |
Aluminum |
Aluminum |
|
Weight (without load distribution bridge) |
2.5 kg |
2.5 kg |
2.5 kg |
|
Weight (with load distribution bridge) |
·/· |
4 kg |
4 kg |
|
Effective span of load distribution bridge |
40 mm |
118 mm |
118 mm |
|
Test load |
Pressure gage 1 |
0 kN … 5 kN |
0 kN … 5 kN |
0 kN … 20 kN |
Pressure gage 2 |
·/· |
0 kN … 25 kN |
·/· |
|
Ambient temperature for operation |
−17 ℃ … 60 ℃ |
−17 ℃ … 60 ℃ |
−17 ℃ … 60 ℃ |
|
Storage temperature |
−20 ℃ … 70 ℃ |
−20 ℃ … 70 ℃ |
−20 ℃ … 70 ℃ |
HAT 28 E |
HAT 28 FX |
||
---|---|---|---|
Maximum displacement |
50 mm |
50 mm |
|
Displacement indicator scale |
mm |
mm |
|
Housing |
Aluminum |
Aluminum |
|
Weight (without load distribution bridge) |
2.5 kg |
2.5 kg |
|
Weight (with load distribution bridge) |
4.5 kg |
·/· |
|
Effective span of load distribution bridge |
207 mm |
40 mm |
|
Test load |
Pressure gage 1 |
0 kN … 30 kN |
0 kN … 30 kN |
Pressure gage 2 |
·/· |
·/· |
|
Ambient temperature for operation |
−17 ℃ … 60 ℃ |
−17 ℃ … 60 ℃ |
|
Storage temperature |
−20 ℃ … 70 ℃ |
−20 ℃ … 70 ℃ |
Operation
Basic test procedure
The commonly used test procedure is described below
- The load distribution bridge is already mounted on the tester. For HAP 2.5 tests, secure the HAP 2.5 load distribution bridge. Be sure to use longer screws (40 mm) to secure this bridge.
- Install the appropriate adapter on the fastener to be tested.
- Application 1: Pass the adapter through the bridge and engage the head centered in the loading claw foot of the tester.
- Application 2: Push the spacer on to the button adapter. Pass the head of the spacer through the bridge and engage the head centered in the loading claw foot of the tester.
- Turn the tester to a position in which the pressure gage is easy to read.
- Adjust the length of the threaded legs to have all three legs in contact with the supporting surface and have the pull-out movement along the axis of the fastener and parallel to the threaded legs.
- Set the red pointer of the gage to zero. Hold the tester by the grip while increasing the load on the fastener by turning the crank clockwise.
- Increase the load until the minimum specified load is attained.
- To relieve the load on the fastener, turn the crank counter-clockwise and push it down until the original state is reached.
- Now remove pull-out tester and adapter.
Use of the spacer
The spacer is used with the button adapters (threaded (A) or slotted (B) ) or for direct testing (without button adapter) of fasteners with a diameter of 16 mm. It consists of a cylindrical section and an M12 threaded rod to which an M12 adapter is mounted. The cylindrical section has a slot into which the adapter for the fastener to be tested fits.One of the load distribution bridges is required for every test using the spacer.
In exceptional cases (e.g. fasteners on steel (X-CRM)), the adapters (M4, M5, M6, M8, M10, M12) can also be used without the spacer for testing.
Under these circumstances, the procedure is the same as that described in the section below for testing with adapters (M12, M16, M20).
Invariably, however, the desired results can be obtained only if the fastener was set correctly prior to installation of the adapter.
Use of the threaded button adapters (M4, M5, M6, M10, M12)
For testing threaded fasteners (for example stud anchors, threaded stud fasteners).Use of the slotted button adapter (4.5 mm, 5.5 mm, 6.5 mm, 8.5 mm, 10.5 mm, 12.5 mm)
For testing fasteners that require a connection to be made to the bolt or anchor head.Use of the threaded rod adapters (M5, M6, M8, M10)
The adapters for M5 and M6 are primarily for testing wall ties.On account of their special shape, the M5 to M10 adapters can be used without the button adapter
Use of the threaded rod adapters (M12, M16, M20)
For testing anchors with external thread or internal thread.For testing an anchor with external thread, the adapter is screwed on to the correctly installed anchor. Screw-in depth: at least equal to thread diameter. The adapter can then be connected directly to the tester.
For testing an anchor with internal thread, a threaded rod is first screwed into the anchor. Then the adapter is screwed on. Screw-in depth: at both ends at least equal to the thread diameter. The adapter can then be connected directly to the tester.
Use of the adapter for X-IE
- Remove the thermal insulation around the fastener.
- Install the pull-out tester together with the adapter. Slip the adapter over the head of the insulating element between the two plates of the X-IE adapter in such a way that the shank of the insulating element engages completely in the hole in the bottom plate.
Testing in restricted spaces
- Unscrew the crank grips.
- You can now turn the crank with a 22 mm ratchet (supplied as part of each kit).
- This facilitates operation when working close to a wall, for example, where there not enough space to turn the crank.
- This facilitates operation when working close to a wall, for example, where there not enough space to turn the crank.
Test of scaffold anchorages
Basic configuration (HAT 28 master kit)
- Unscrew the swiveling feet from the threaded-rod legs.
- Remove the threaded-rod legs.
- Screw the 100-mm hex legs into the bridge and tighten until hand-tight.
- If necessary, screw the 50-mm hex legs into the 100-mm hex legs and tighten until hand-tight.
- Screw the swiveling feet to the ends of the legs.
- Check that the pin of the ringbolt adapter is secured with the chain to the adapter itself.
- Screw an M12 threaded button adapter or the M12 locking adapter on to the threaded rod of the ringbolt adapter and engage the latter in the loading claw foot of the tester.
- If the surface is uneven, compensate by precision-adjusting the legs before proceeding with the test.
Use of the scaffold ringbolt adapter
- Remove the pin from the adapter and position the adapter over the scaffold ringbolt. Reinsert the pin into the adapter and through the scaffold ringbolt.
Bridge installation, HAT KIT HAP 2.5
- Lay the HAT 28 on its side.
- Using the screwdriver supplied, remove the two hex socket screws (length with head 35 mm) that connect the HAT 28 to the standard bridge.
- Lay the standard bridge in the case of the HAT 28.
- Remove the large bridge from the case of the HAT KIT HAP 2.5.
- Lay the large bridge on its side.
- Remove the two longer screws (length with head 50 mm) from the case of the HAT KIT HAP 2.5.
- Using the screwdriver, screw the HAT 28 with these longer screws to the HAT KIT HAP 2.5.
- Using the screwdriver, tighten the screws until the tester no longer wobbles.
HAP 2.5 tests
- Using the pins and holes in the legs, set the large bridge to the correct height.
- Remove the pin from the adapter.
- Position the connecting disk inside the adapter.
- Re-insert the pin into the adapter through the connecting disk.
- Pass the power cord of the HAP 2.5 over the connector disk.
- Push the pin back into the adapter.
Test of welded studs
- Screw a threaded button adapter on to the F‑BT stud.
- Engage the latter in the loading claw foot of the tester.
- If necessary, for a long stud use a spacer see the overview of spacers.
Care and maintenance
Care- Carefully remove stubborn dirt from the tool.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
- Frequent removal and reconnection of the pressure gage causes the oil level in the reservoir to drop. In extreme cases this can result in the volume of oil dropping below the level necessary for the pressure gage to show a correct reading.
Technical data X > 6 mm … < 15 mm - When this happens, it is advisable to bring the tester to a Hilti repair workshop for checking and refilling with oil.
Transport and storage
- Store the product in a dry place, where it cannot be accessed by children or unauthorized persons.
- Check the product for damage before use after long periods of transport or storage.
Disposal
Most of the materials from which Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
For more information on operation, technology, environment and recycling, follow this link: qr.hilti.com/manual?id=286175This link is also to be found at the end of the documentation, in the form of a QR code.